Part Number: TXS0202
I'm using TXS0202YZPR in the project. The A-voltage is 2.5V and B is 3.3V. When set high level on the D-(A) and D+(A), i see that D-(B) is 3.3V, but D+(B) is about 2.0V. I've tested it on two boards. What is the reason? Schematic:
This is D-
D+ is:
Best regards.