Hi team,
Some questions from my customer evaluating LSF0204 in the design as I2C level shifter (also isolation).
1. As the EN follow the logic of VrefA, will there be leakage from An to Bn if we only pull-high Vrefn (and leave VrefB 0V)?
2. If customer also plans to use LSF0204 as the GPIO level shifter, where the GPIOs are push-pull outputs, do we need the external pull-high voltage rail any more? Or we need pull-high on the Bn side only when An side is push pull GPIO output?
Thanks
Max