Part Number: MSP432P401R
Some details are being taken with the MSP432P401R microcontroller, since some of our devices that have this microcontroller are blocking (after a while the programming stops executing), even though they have the Watchdog activated and configured so that in case of failure the microcontroller restarts, we hope to see if they could give us support, since as it is not presented in all devices, we have the doubt if it could be our PCB, something in programming or already in itself that the microcontroller is failing, since even charging the program again, it is always presented on the same devices.