Part Number: EK-TM4C129EXL
Dear Sir,
I have problem during debugging , I have some error when I take example project event-ek-tm4c129exl-ti. Error is given below
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: EK-TM4C129EXL
Dear Sir,
I have problem during debugging , I have some error when I take example project event-ek-tm4c129exl-ti. Error is given below
Did you get the following output on the console before the program terminated?
writing message id = 0 val = 'a' ... writing message id = 1 val = 'b' ... writing message id = 2 val = 'c' ... Implicit posting of Event_Id_02 read id = 0 and val = 'a'. Implicit posting of Event_Id_02 read id = 1 and val = 'b'. writer done. Implicit posting of Event_Id_02 read id = 2 and val = 'c'. Explicit posting of Event_Id_00 and Implicit posting of Event_Id_01 writing message id = 0 val = 'a' ... writing message id = 1 val = 'b' ... writing message id = 2 val = 'c' ... Implicit posting of Event_Id_02 read id = 0 and val = 'a'. Implicit posting of Event_Id_02 read id = 1 and val = 'b'. writer done. Implicit posting of Event_Id_02 read id = 2 and val = 'c'. Explicit posting of Event_Id_00 and Implicit posting of Event_Id_01 writing message id = 0 val = 'a' ... writing message id = 1 val = 'b' ... writing message id = 2 val = 'c' ... Implicit posting of Event_Id_02 read id = 0 and val = 'a'. Implicit posting of Event_Id_02 read id = 1 and val = 'b'. writer done. Implicit posting of Event_Id_02 read id = 2 and val = 'c'. Explicit posting of Event_Id_00 and Implicit posting of Event_Id_01 writing message id = 0 val = 'a' ... writing message id = 1 val = 'b' ... writing message id = 2 val = 'c' ... Implicit posting of Event_Id_02 read id = 0 and val = 'a'. Implicit posting of Event_Id_02 read id = 1 and val = 'b'. writer done. Implicit posting of Event_Id_02 read id = 2 and val = 'c'. Explicit posting of Event_Id_00 and Implicit posting of Event_Id_01
If you did, the program executed properly and then called BIOS_exit from the task "readertask". By default Code Composer sets a breakpoint at the program termination point which is a branch to self shared by the abort routine. If you don't want a breakpoint there, you can disable it from the "Tools" -> "ARM Advanced Features", "Program/Memory Load Options" menu.

Dear Bob,
My consol output like that
Enter swi0Fxn, a0 = 1, a1 = 0
swi0 trigger = 0
swi0 pri = 2
Exit swi0Fxn
Enter swi1Fxn, a0 = 2, a1 = 0
swi1 trigger = 3
swi1 pri = 1
Exit swi1Fxn
Running tsk0Fxn
Enter swi0Fxn, a0 = 1, a1 = 0
swi0 trigger = 2
swi0 pri = 2
Exit swi0Fxn
Enter swi1Fxn, a0 = 2, a1 = 0
swi1 trigger = 259
swi1 pri = 1
Exit swi1Fxn
Enter swi1Fxn, a0 = 2, a1 = 0
swi1 trigger = 0
swi1 pri = 1
Exit swi1Fxn
Enter swi1Fxn, a0 = 2, a1 = 0
swi1 trigger = 0
swi1 pri = 1
Exit swi1Fxn
Calling BIOS_exit
What can I do?
Thanks
Imtiaj
That output is not from the project "event-ek-tm4c129exl-ti", but rather from the project "swi-ek-tm4c129exl-ti". The output is correct for that project.