Part Number: TM4C129XNCZAD
In our new project we are planning to use the internal RTC of the TM4c129X , currently we use BQ32000DR with 32.768 Crystal along with 3.0VDC battery(BR-2032/HEN).
For using the internal RTC of TM4c129x we want to know the power requirements of the controller in the Hibernation mode so that we can perform the battery life calculation. (I tried searching in the datasheet but was not able to find it)
Also we want to know if external RTC is recommended over the internal RTC of controller , what will be the trade off in doing so. We have energy meter application where the correctness of the RTC is critical along with the battery life.
Your are requested to kindly address the issue.
Thanks and Regards,
Abhijit Kumar