This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-TMS57004: XSD100 v2 Required dynamic library jscserdes could not be located.

Part Number: LAUNCHXL-TMS57004


I have found this in a number of forum posts, but they are all locked.

When testing a Hercules TMS04 Launchpad with and XDS100v2 debugger, it fails. From CCS V10 and from command line.

My CCS is installed here: D:\ti\ccs1010

My board file is located here: C:\Users\jancu\AppData\Local\TEXASI~1\CCS\ccs1010\0\0\BrdDat\testBoard.dat

When navigating to D:\ti\ccs1010\ccs\ccs_base\common\uscif , then executing 

dbgjtag -f C:\Users\jancu\AppData\Local\TEXASI~1\CCS\ccs1010\0\0\BrdDat\testBoard.dat -rv -o -F inform,logfile=yes -S pathlength -S integrity

I get the error here:

D:\ti\ccs1010\ccs\ccs_base\common\uscif>dbgjtag -f C:\Users\jancu\AppData\Local\TEXASI~1\CCS\ccs1010\0\0\BrdDat\testBoard.dat -rv -o -F inform,logfile=yes -S pathlength -S integrity

-----[Print the board config pathname(s)]------------------------------------

C:\Users\jancu\AppData\Local\TEXASI~1\CCS\
ccs1010\0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioserdesusb.dll'.

An error occurred while soft opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-716' (0xfffffd34).
The title is 'SC_ERR_LIB_LOAD_SERDES_DRV'.

The explanation is:
Required dynamic library jscserdes could not be located.
The library isn't on the search path.

The DLL exists, and is in the working folder.

01-01-2021  22:30           106 496 jscserdes.dll

Other posts are locked because the OP did not reply. I will reply.