Part Number: TM4C1230C3PM
Hello guys ,
I am looking to be able to update a Tiva TM4C1230C3PM with a new bin file. To do this I am trying to find a host tool that I can call from a bash script that will then send a .bin file over to a tiva , via uart, from TM4C1230C3PM where the uart flash bootloader on the tiva will take over and actually flash the device.
I've implemented the TI flash based boot loader and allocated memory accordingly in the .cmd file. My application starts at 0x1000 so that the bootloader has 0x000~0x1000. I have used lm flash to flash both the bootloader and the main application with success. Now I just need to figure out how to update a .bin file over from a linux(debian) computer.
do you know if exist any program or tool that allows me to load .bin to the tiva via uart ? using linux