Part Number: TMS570LS3137
Other Parts Discussed in Thread: HALCOGEN
Hello,
When using the PBIST module, after:
- Setting the clock divider with the ROM_DIV to have 50 MHz PBIST clock frequency
- Enabling PBIST controller with MSIENA=1
- Enabling PBIST self-test with MSTGENA=0xA
- As soon as the the PBIST internal clock is enabled with PACT=1
- The registers FSRDL0=FSRDL1=0xaaaaaaaa; RINFOL=RINFOU=0xFFFFFFFF and can no longer be modified by the application, forcing all RAM/ROM groups to be tested and failed.
How may I change RINFOL and RINFOU registers with selected RAM/ROM groups for test?
Thanks.