This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSRM48HDK: How to burn the compiled bin file to the development board through RJ45 connection

Part Number: TMDSRM48HDK

[What I need?]

Our company is tring to set up a CI/CD pipeline and needs to download our software to the development board via Internet cable.

[What I 've done?]

I have turned on the s2:4 network switch on the development board and connected the board into our LAN.

I looked up the ip address of the board from the backstage of the router. And I can ping the board from my windows computer.

I have already tested download softwar via JTAG with a arm emulator using JFlash.

I cann't establish a connection in JFalsh with TCP/IP.

What should I do next?