Part Number: MSP432P401R
Other Parts Discussed in Thread: BOOSTXL-SHARP128, MSP430F5638, MSP-EXP430F5529LP, MSP430WARE
Currently have the BOOSTXL-SHARP128 booster pack running on the MSP-EXP432P401R Launch Pad.(Rev 2.1). Both the fatsd and fatsdraw example projects build and are running. I can read / write to a 32 GB microSD card inserted into the booster pack successfully.
I need to port this example code to a custom SBC running an MSP430F5638 which is interfaced to a microSD card socket via SPI. A possible intermediate step would be getting the booster pack and code running on either a MSP-EXP430F5529LP or MSP-EXP430G2ETLP which I have.
So far, I've copied the 432 fatsd and fatsdraw projects into a 430 Workspace and changed the MCU in the Project settings from 432 to 430. When it builds it can't find the following:
NoRTOS.h
third_party\fatfs\ffcio.h fixed this by copying the fatsd folder into the new Workspace, and add files to project
ti\drivers\Display.h
ti\drivers\dpl\Semaphore.h
C:\ti\simplelink_msp432p4_sdk_3_40_01_02 Looking under 432, I can find all of these missing files
C:\ti\msp430ware_3_80_13_03\ Looking under 430, I don't see any of the missing files
So where are these missing files for a 430, and how do I complete the port?