Part Number: TMS570LS3137
Dear all,
we tried to read back the program field and the control field of the N2Het from the instruction RAM for verification purposes. Reading back these fields seems to have an impact on the data field.
We are using the CNT instruction and the ECNT instruction in the N2Het.
We feed in constant pulse counts, read after a fixed time (5ms) and expect a constant increase in the value in the data field. When we read the program field and the control field, the data field contains unexpected (seems like it might be "old") values. When reading back the program and control field just every couple of cycles, the incremented value is correct. I.e. the value is once too low and once too high but in total after a while everything is correct. When we are not reading the program and control field, everything works as expected.
Is it possible to read back program field and the control field without an effect to the data field?
Thank you and best regards,
Philipp