Part Number: TM4C1297NCZAD
HI,
I have a fan that is connected to PWM
At some point of time, i would like to turn off the PWM before going idle mode. I cant find a way to disable it.
This is how i configured it
GPIOPinConfigure(GPIO_PD0_T0CCP0);
GPIOPinTypeTimer(GPIO_PORTD_BASE, GPIO_PIN_0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);
TimerConfigure(TIMER0_BASE, TIMER_CFG_SPLIT_PAIR|TIMER_CFG_A_PWM);
TimerLoadSet(TIMER0_BASE, TIMER_A, 4000);
TimerMatchSet(TIMER0_BASE, TIMER_A, 1000);
TimerEnable(TIMER0_BASE, TIMER_A);
I have tried using TimerDisable (TIMER0_BASE, TIMER_A); but it does nothing.
The closest i have tried and worked is (this is absolutely embarrassing to use :) )
TimerLoadSet(TIMER0_BASE, TIMER_A, 4000);
TimerMatchSet(TIMER0_BASE, TIMER_A, 3999);
I read in other post that TIVA does not accept 0% duty cycle.
Is there any graceful a.k.a proper way to do this?
Thanks in advanced.