Part Number: TMS570LS1227
I do many re-flashing now while debugging and i've started to hit this problem too often - code gets stuck on boot in this section:
/* Check if there were ESM group3 errors during power-up.
* These could occur during eFuse auto-load or during reads from flash OTP
* during power-up. Device operation is not reliable and not recommended
* in this case.
* An ESM group3 error only drives the nERROR pin low. An external circuit
* that monitors the nERROR pin must take the appropriate action to ensure that
* the system is placed in a safe state, as determined by the application.
*/
if ((esmREG->SR1[2]) != 0U)
{
/* USER CODE BEGIN (24) */
/* USER CODE END */
/*SAFETYMCUSW 5 C MR:NA <APPROVED> "for(;;) can be removed by adding "# if 0" and "# endif" in the user codes above and below" */
/*SAFETYMCUSW 26 S MR:NA <APPROVED> "for(;;) can be removed by adding "# if 0" and "# endif" in the user codes above and below" */
/*SAFETYMCUSW 28 D MR:NA <APPROVED> "for(;;) can be removed by adding "# if 0" and "# endif" in the user codes above and below" */
for(;;)
{
}/* Wait */
/* USER CODE BEGIN (25) */
/* USER CODE END */
}
I don't think there is actual hw error, or it shouldn't be .. At the same time, I didnt' see any comments that this test should be disabled while debugging.
Any idea whats happening? Today/now i can't get passed it, might need to power cycle the board, as no amount of debug restarts help seems.