Part Number: MSP432E401Y
Other Parts Discussed in Thread: UNIFLASH,
I can successfully program my MSP432E401y using uniflash 6.0.0 GUI. I can also program the MAC address register using the uniflash GUI. I then generate an "install package" using the Standalone Command Line. When I run the generated installer (DSLite.bat), it programs the flash, but does not program the MAC Address. I've tried performing a device unlock before calling dslite.bat, but it still does not work. I'm using the uniflash GUI "Read MAC Address" to verify the MAC address contents.
DSLite has the MAC address I wish to program in the user_files/settings/generated.ufsettings file:
type user_files\settings\generated.ufsettings
{"Texas Instruments XDS110 USB Debug Probe/CORTEX_M4_0":{"FlashMACAddrInput":"00-00-60-01-02-03"}}
when I run dslite I get the following output:
dslite.bat
Executing default command:
> dslite --mode flash -c user_files/configs/msp432e401y.ccxml -l user_files/settings/generated.ufsettings -s VerifyAfterProgramLoad="No verification" -e -f -v "user_files/images/flash1_00-00-01-00.out" "user_files/images/flash2_00-00-01-01.out"
DSLite version 10.1.0.1986
Configuring Debugger (may take a few minutes on first launch)...
Initializing Register Database...
Initializing: CS_DAP_0
Executing Startup Scripts: CS_DAP_0
Initializing: CORTEX_M4_0
Executing Startup Scripts: CORTEX_M4_0
Connecting...
CORTEX_M4_0: GEL Output:
Memory Map Initialization Complete
Loading Program: Multiple Files
Preparing ...
.text: 0 of 5376 at 0x0
.text: 0 of 39840 at 0x3000: 11%
.text: 32640 of 39840 at 0x3000: 84%
Finished: 84%
Setting PC to entry point.: 84%
Verifying Program: Multiple Files
Preparing ...
.text: 0 of 5376 at 0x0
.text: 0 of 39840 at 0x3000: 11%
.text: 32640 of 39840 at 0x3000: 84%
Finished: 84%
info: CORTEX_M4_0: Program verification successful for Multiple Files
Running...
Success
After the programming is complete I use the uniflash GUI's read mac addess operation, and it still reports the MAC address as FF-FF-FF-FF-FF-FF.
Can you please tell me how I can make this work?