Hi Experts,
The Safety Manual mentions the Diagnostic RST1 "External Monitoring of Warm Reset (nRST)" as way to signal an external monitor, that a Reset has been generated.
In our Application we want to use the J2 Pin as a second nERROR to signal external Hardware to enter Safe State instead. If I understand correctly the J2 pin will become GIOB[6] (Input Pull-Down) on warm reset, which can also be used to signal to external hardware, that a reset has occured.
(Q1) Can the reset state of the pins (e.g. J2) be influence by an external source (e.g. Clock failure...)?
(Q2) Is it absolutely necessary to use the nRST to establish the safe state in the peripherals?
Thank you and best regards,
Max Wittekind