Part Number: TMS570LC4357
Hi experts,
we want to use the Pins of the RTP and DMM-Modules as GPIO, but the Safety Manual mentions safety measure DMM1 "Disable the DMM Pin Interface" and RTP1 "Disable the RTP Pin Interface"
Furthermore the manual states in section 6.39.1:
"For the purposes of FIT estimations and safety use, this module is considered strictly as a Debug/Trace related module and active use during an application runtime is not considered even if used solely as GPIO"
(Q1) Should the RTP and DMM Pins not be used or is there way that would allow us to use the Pins as GPIO?
Thank you and best regards,
Max