Part Number: MSP432E401Y
Hello,
Is it possible to update the MSP432E401Y's firmware via UART4 (instead of the default UART0) ?
If yes, how to do so ?
Thank you.
Regards,
Victor Tolosana
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP432E401Y
Hello,
Is it possible to update the MSP432E401Y's firmware via UART4 (instead of the default UART0) ?
If yes, how to do so ?
Thank you.
Regards,
Victor Tolosana
You can't use the default bootloader via UART4. Maybe you need a customized one.
Ok, by that you mean modifying bl_uart.h in boot_serial_uart_flash_MSP_EXP432E401Y_nortos_ccs ?
Changing all #define with adequate pins for UART4 should make it work ?
Thank you very much.
You can see that the default bootloader is in ROM:

The one you find is an Application bootloader saved in flash. You can customized it as what you want.