Part Number: RM46L852
Dear
I want to use the motor encoder and hall sensor inputs on RM46L852.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: RM46L852
Dear
I want to use the motor encoder and hall sensor inputs on RM46L852.
Hello Chunho,
You can use either N2HET port or ETPWM ports to generate PWM signal for motor control, and use N2HET or ECAP to capture input signals. RM46 has two build-in 12-bit ADC modules to sample the current or voltage.
The series resistor is used as terminator to reduce the signal reflection.
Dear Wang
Thanks for your reply!
Does this mean that the N2HET and ECAP ports can accept Hall sensor and encoder inputs?
Is it not necessary to use the eQEP port for encoder input?
And two port(ECAP5 and ETPWM7A) is used as one input(ETPWM7A) in your reference schematic.
Wye use two port as one input?
And two port(ECAP5 and ETPWM7A) is used as one input(ETPWM7A) in your reference schematic.
Wye use two port as one input?
The control was developed for two different base boards which have different pinout for J1 connector. For DRV803x RevB EVM, the J1 pin 30 and pin 80 are used to capture HALL sensor signals and routed to ECAP5 and ECAP6.
Does this mean that the N2HET and ECAP ports can accept Hall sensor and encoder inputs?
You can use either ECAP or N2HET to capture HALL sensors' signals. The N2HET can also be programmed to act as EQEP.
Is it not necessary to use the eQEP port for encoder input?
You don't have to use eQEP. But it is easier to use ECAP and eQEP than using N2HET.