Part Number: TMS570LS1224
Hi Team,
Our customer would like to confirm about the analog input clamp current stated in the datasheet and errata.
I am using TMS570LS1224 and in the datasheet the information about "Analog input clamp current" is, that it is some value when input voltage exceeds Vccad + 0,3V. In Errata there is some additional information about injecting current into an input channel and it says that it happens when the input voltage exceeds Vccad - 0,3V....
I would like to make sure that the info in Errata is correct and it is really Vccad - 0,3 V and not Vccad + 0,3V. Could you advise on that?
Thank you for your support!
Regards,
Danilo