Part Number: EK-TM4C1294XL
Dear Sir/Madam,
I am using EK-TM4C1294XL board. In my application I am using ADC input AIN1,AIN2,AIN3,AIN5,AIN6,AIN7.
I want to read all the ADC data in interrupt.
I have installed TI-SDK and checked the sample below,
ti\TivaWare_C_Series-2.2.0.295\examples\boards\ek-tm4c1294xl\adc_udma_pingpong
ti\TivaWare_C_Series-2.2.0.295\examples\peripherals\adc
from that I got DCSequenceStepConfigure(ADC0_BASE, 0, 0, ADC_CTL_CH0 | ADC_CTL_END | ADC_CTL_IE); - based on ADC_CTL_CH0 it will select channel
IntEnable(INT_ADC0SS0); - common to enable the all ADC0 interrupt
ADCSeq0Handler() - single handler for all ADC0 interrupt.
if it is a single handler how to identify which channel the interrupt arrived.
Kindly help.
Thanks