Part Number: TMS570LS0232
Where can i find this parameter?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
MTTFd (Mean time to dangerous failure) is used in ISO13849.
The metrics listed in our FMEDA is for IEC61508 and ISO26262. You can use those data to estimate the parameters for ISO 13849.
IEC 61508 offers 4 Safety Integrity Levels (SIL) for safety related systems: SIL1, SIL2, SIL3, and SIL4. The SIL classification of safety related systems depends on the following parameters:
ISO 13849 offers 5 categories (Cat) and 5 performance levels (PL): CAT B, CAT 1,...CAT 4; PL a, PL b,... PL e
Normally the following parameters are used in ISO 13849 when assigning CAT and PL level to a safety related system:
ISO 13849 uses MTTFd for quantifying channel safety, and PFH for quantifying safety of the complete safety related system. You can estimate the MTTFd as 1/PFH.
Please refer to the spec of ISO 13849.
These documents are available on the safeTI forum, as they can only be accessed under the safeTI NDA.
This page has links to all safety-related NDA documentation (requires safeTI NDA for access): e2eprivate.ti.com/.../1105.aspx
Please contact with TI local sales or FAE if you don't have Safeti NDA.