Part Number: TMS570LC4357
Sir/madam,
I've been using the TMS570LC4357 for a while.
I'd like to add NOR flash via the EMIF.
I'm looking at a Cypress NOR flash parts
Q: the EMIF has 22 address bits..and 16 data bus bits....so, I could hook up a 128Mbit , (16data bits, 0-22 address) directly...correct?
using multiple chip selects, I could add more memory across the EMIF (i.e. as shown in SPNU563A–March 2018, page 841)..correct?
just wnat to make sure I hook it up correclty...I dont have a lot space on teh pcb, so Qty1 NOR flash as described above would be suffiicicnt...
is there any other doc/reference/eval board that shows proper connection of a NOR flash (as described) to the EMIF of the Herc?
thank you for all your help!