Part Number: TMS570LC4357
Hello,
I am using DMA to get data from an external device connected to SCI3. To the best of my understanding (and according to the nice example https://www.ti.com/lit/an/spna213/spna213.pdf), the DMA "reads 32 bits at a time from the data RAM incrementing the address". Nevertheless, the data in my desination address is always 3 bytes of 0 and 1 byte of (correct) data.
For example, if the external device sends 0x3A45B, the desination address gets {0x0, 0x0, 0x0, 0x3, 0x0, 0x0, 0x0, 0xA, 0x0, 0x0, 0x0, 0x4, 0x0, 0x0, 0x0, 0x5, 0x0, 0x0, 0x0, 0xB};
I tried playing aroung with the parameters -mainly Read and Write sizes and offsets- but I fail to make it transmit all 32 bits of actual data.
Is there a way for the DMA to transmit all 32 bits from SCI?
Mysetup:
#define FRAME_TRANSFER 5 dmaCTRLPKT_RX.SADD = (uintptr_t) &(sciREG3->RD); /* source address */ dmaCTRLPKT_RX.DADD = (uintptr_t) shared_mem_p; /* destination address in shared RAM */ dmaCTRLPKT_RX.ELCNT = 1; /* element count */ dmaCTRLPKT_RX.CHCTRL = 0; /* (channel control) bufferId */ dmaCTRLPKT_RX.FRCNT = FRAME_LENGHT; /* frame count */ dmaCTRLPKT_RX.ELDOFFSET = 0; /* element destination offset */ dmaCTRLPKT_RX.ELSOFFSET = 0; dmaCTRLPKT_RX.FRDOFFSET = 0; /* frame destination offset */ dmaCTRLPKT_RX.FRSOFFSET = 0; /* frame source offset */ dmaCTRLPKT_RX.PORTASGN = PORTB_READ_PORTA_WRITE; dmaCTRLPKT_RX.RDSIZE = ACCESS_32_BIT; dmaCTRLPKT_RX.WRSIZE = ACCESS_32_BIT; dmaCTRLPKT_RX.TTYPE = FRAME_TRANSFER; /* transfer type */ dmaCTRLPKT_RX.ADDMODERD = ADDR_FIXED; /* address mode read */ dmaCTRLPKT_RX.ADDMODEWR = ADDR_INC1; /* address mode write */ dmaCTRLPKT_RX .AUTOINIT = AUTOINIT_OFF; /* autoinit
Cheers,
Arturo.