Part Number: TMS570LC4357
This is with reference to the previous discussion https://e2e.ti.com/support/microcontrollers/other-microcontrollers-group/other/f/other-microcontrollers-forum/995129/tms570lc4357-mibspi-with-dma-buffer-transfer-cs-issue.
The MibSPI and DMA transfer are stable at 15MHz clock frequency with big data buffer (E_COUNT 64 and F_COUNT 4 )
Using update mode as 5 with BTC interrupt to initiate TX.
with 20MHz clock the frame overlap observed. Please refer the previous discussion for details.
Few questions asked in the previous discussion, which are not yet answered. Request to provide your observations.
1.When the BTC interrupt was hit, I am reconfiguring the DMA channel to trigger TX. May be this is not correct. Please let me know, what is the proper method.
2.To synchronize the TX and RX between both the channels I am using buffer mode as 5 (Wait until TX full). Please note that my communication is between two different controllers, and I need to create mirror image of global data buffer with least possible latency. Shall I need to use different buffer mode for proper sync.
3.What is the highest clock speed can be used practically with MibSPI.
4.I am using motor control FOC in the ETPWM interrupt, which was configured for 25 KHz cycle time. Do this interrupt have any impact on the DMA transfer?
Thanks. Chandra