Part Number: TMS570LS3137-EP
Other Parts Discussed in Thread: HALCOGEN
Hi,
I enabled EMAC internal loopback and configured Tx packet of 142 bytes with broadcast enabled. Though I could observe the Transmission status in EMAC registers, I am not able to receive the packets. The packet is getting filtered.
On the Tx side after transmitting one packet frame:
TXGOODFRAMES - 0x00000001
TXBCASTFRAMES - 0x00000000
TXOCTETS - 0x00000092
FRAME128T255 - 0x00000001
NETOCTETS - 0x00000124
On the Rx Side:
RXFILTERED - 0x00000001
RXGOODFRAMES - 0x00000000
RXBCASTFRAMES - 0x00000000
RXOCTETS - 0x00000000
Could you please help to resolve this issue?
Also, I couldn't see register contents of following registers even with debugger HALTED. I am seeing the message "Error: Unable to read"
Starting from
500h MACADDRLO MAC Address Low Bytes Register
....
....
67Ch RX7CP Receive Channel 7 Completion Pointer Register
I am using CCS 10.1.1. Please help to resolve this issue.
This is sample code
//Destination address
for(i=0;i<6;i++)
EthernetTestData[i]=0xFF;
//Source address
EthernetTestData[6]=0xFF;
EthernetTestData[7]=0xFF;
EthernetTestData[8]=0xFF;
EthernetTestData[9]=0xFF;
EthernetTestData[10]=0xFF;
EthernetTestData[11]=0xFF;
// LEN = 128 bytes
EthernetTestData[12]=0x00;
EthernetTestData[13]=0x80;
//Data bytes
for(i=14;i<142;i++)
{
EthernetTestData[i]=i;
}
MyPacket.next = NULL_PTR;
MyPacket.payload = &EthernetTestData[0];
MyPacket.tot_len = 142;
MyPacket.len = 142;
EMACTransmit(hdkif, &MyPacket);
Thanks,
Jai