Part Number: MSP432P401M
The I/O pins associated with HFXT (J2 and J3) and 4-wire JTAG (J4 and J5) can be used as GPIO if those features are not needed in a system. The device H/W fully supports this functionality but the TI PinMux tool on dev.ti.com (SysConfig (1.8.1+1900)) lists these pin configurations as N/A and does not allow the pins to be configured as GPIO.
Can this limitation of SysConfig (1.8.1+1900) be fixed or are there any workarounds available besides manually editing the output files?