This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EK-TM4C1294XL: Unable to launch CCS debug session

Part Number: EK-TM4C1294XL

Hello E2E,


Our customer is encountering the error below when opening a new CCS project and want to start debugging. Need your help with the workaround on the error. Thank you.



Regards,
Carlo

  • The error message is saying that there is no target configuration file associated with the new project. There are several ways to correct this. One is to right click on the project in the "Project Explorer" window and select "Add Files...". Now you search for a target configuration file appropriate for your Lauchpad. Search to "C:\ti\TivaWare_C_Series-2.2.0.295\examples\boards\ek-tm4c1294xl\project0\ccs" and select the file "target_config.ccxml". (These example projects are part of TivaWare. If the customer has not already downloaded TivaWare, they should do that first.) Now when the project is launched it will know what target configuration to use.

    To avoid this issue in the future, it is best to start a new project by importing an example project from TivaWare and renaming it. I often use the "project0" referenced above when starting a new project with the EK-TM4C1294XL Launchpad.