Part Number: TMS570LS3137
Hello.
I resort to making a query, since I am stuck on my project.
I am working with the TMS570, in a program with RTOS.
I implemented the use of lwIp 1.4.1, to be able to make a TCP client in my project. To use that library with FreeRTOS, they recommended that I use the Netconn APIs.
The problem is that when I want to use them, I get several header errors.
In lwipopt.h I made the change to: NO_SYS 1 and LWIP_NETCONN 1
At the beginning my project told me these errors:

I define them in sys_arch, but then I get the following errors:

The truth is I don't know how to solve this. Please, if anyone knows how to be able to use the lwIP APIs for FreeRTOS with the TMS570 I would be very grateful if you would share it.
What I need are the sys_arch.c files to be able to use the API.