Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53513RVER

Other Parts Discussed in Thread: TPS53515, TPS53513

Dear Supplier,
-The mentioned part number has the same chemical composition as TPS53513RVER but one of them is RoHS compliant and the other one isn't compliant. Can you please provide clarification regarding this difference?

-As I checked the chemical composition before, I saw the 7a exemption which is related to the amount of Lead while these two products have the same amount of Lead in their chemicals composition and one of them is not compliant with RoHS regulation. Can you please explain this for me?
Ref.


TPS53513RVER
TPS53513RVET


Regards,
Amin Nikpayam

Junior Project Manager

  • TPS53513RVER and TPS53513RVET are the same device.   The T are R suffixes are the package quantity.   Both should be RoHS-Exempt & Green.

    The TPS53515 is a very similar device only the current rating is different,   Both T and R are RoHS-Exempt & Green in that datasheet.

    I have asked the documentation team to correct the TPS53513 datasheet.