Part Number: MSP-EXP432P401R
I installed a copy of Code Composer Studio 10.3 on a Linux host. Then, I connected my board MSP-EXP432P401R to its through USB cable. When I tried to test the connection to my board, it failed.
How do I correct it?
[Start] Execute the command: %ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity [Result] -----[Print the board config pathname(s)]------------------------------------ /home/timmy/.ti/CCS10/0/0/BrdDat/testBoard.dat -----[Print the reset-command software log-file]----------------------------- This utility has selected a 100- or 510-class product. This utility will load the adapter 'libjioxds110.so'. The library build date was 'Apr 29 2021'. The library build time was '17:46:08'. The library package version is '9.3.0.00058'. The library component version is '35.35.0.0'. The controller does not use a programmable FPGA. An error occurred while hard opening the controller. -----[An error has occurred and this utility has aborted]-------------------- This error is generated by TI's USCIF driver or utilities. The value is '-600' (0xfffffda8). The title is 'SC_ERR_LIB_ANY_LOCATE'. The explanation is: A required dynamic library could not be located. The library isn't on the search path. [End]