Part Number: TM4C129XNCZAD
Hi..
Connecting an SRAM chip to the EPI pins and just want to confirm I understand the pins assignments (chip manual) correctly(ADDR 11 pins, data 15 bits, WR,RD and CS.
EPI0S0:15 can before D0-D15
EPI0S16:27 can before A0-A11
EPI0S28 RD
EPI0S29 WR
Depend on CS used and config
EPI0S27 can be CS0 or CS1
EPI0S33 can be CS3
EPI0S34 can be CS2
Does the above pin assignment look correct?
In addition, is the an specific application report on this interface and example code as well?
Thanks in advance!
Rob