Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: UNIFLASH, EK-TM4C1294XL
Greeting for the Day,
I am working on enet_io example program Tivaware library. This application works fine on TM4C1294XL evaluation kit.
Now I want to implement same application on a customized board which has TM4C1294NCPDT microcontroller and the ethernet port is connected to same pins as in evaluation kit. But when I connect the ethernet cable from the customized board to computer, the ethernet port is not detecting.
Do I need to add any extra lines in the program so that my issue will be resolved. If so then what should I add in enet_io program
Kindly give me a solution for this.
Part No: TM4C1294NCPDT
Thank you.