Part Number: TMS570LC4357
working with the TMS5704357BZWTQQ1
Question:
I see certain pins and their description..example:
MIBSPI3CLK/AD1EXT_SEL[1]/eQEP1A, Pin V9..description: I/O Pullup Programmable, 20 μA 8mA MibSPI3 clock, or GIO.
the question...
so, can this pin be programmed as a general purpose I/O...(i.e. like use it to turn an LED on off, or read a digital switch input high or low)???
or
it only has the functions associated with the description (i.e. SPI clk out, external mux select outputt, Enhanced QEP1 Input A, )...?
thank you for responding...appreciate the education.