This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ARM-CGT: Porting from a minGW project into a ARM-CGT-CLANG-1_1.3.0.LTS

Part Number: ARM-CGT


Hi,

what would be the best approach to port a pre-existing minGW project into a ARM-CGT-CLANG-1_1.3.0.LTS?

More details: the project was previously build and compiled in Vanilla eclipse and i would like to port it into another target for which i require CLANG-1_1.3.0.LTS.

CCS Ver : 10.3.1.00003 

Eclipse Ver: 2021-06 (4.20.0)

currently when i add the project to CCS i cannot find an option to change the toolchain into CLANG-1_1.3.0.LTS.

i looked in project Properties screen but the "CCS General" tab is missing.

When adding the project to Eclipse and going to project "Properties ->C/C++ Build -> Tool Chain Editor "  there is no option to select or add the CLANG-1_1.3.0.LTS toolchain.

Thank you.