Part Number: TMS570LS3137
1.What's the exact meaning of RDS? RDS is one of the information about self-test failure,value of it despends on RGS.
2.As described in manual, "resume the test if required using Program Control register(offset = 0x16c) STR = 2." So, where is the Program Control register? I searched the whole manual ,but failed.
3.In Fail Status ** Register description,what's the exact menaning of port0 and port1 ? refer to single port and dual port? So, why only port0 Fail Status Fail Register? port1 failure?
4.In table 2-5, why lack of RGS and RDS about FLEXRAY when it in RAM Group 17?Why lack of the grouping information about TCRAM?According to number, whether lack of ESRAM?
Thanks.