This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: 01252018I6

Part Number: TMS570LC4357
Other Parts Discussed in Thread: UNIFLASH

Hello,

I've following all the steps that your propose here:

  1. From the View menu in CCS open the Target Configuration View
  2. Find the .ccxml file that is part of your project
  3. Right click on it and choose "Launch selected configuration".  This will start a debug session in CCS but won't connect to anything yet.
  4. When the debug view opens click on the top level node in the tree (it will be the name of the .ccxml file).  Select "Show all cores".
  5. Under "Non debuggable devices" select the one that ends in ICEPick_C.
  6. Click on the connect button on the toolbar. 
  7. Open the registers view.
  8. If you expand core registers. Do the TAP registers have values other than 0 or 1?
  9. Next select the DAP under "Non debuggable devices" and see if you can connect to that.
  10. After DAP is connected, open CCS Memory Browser to check the value at 0xFFFF_E1E8 (SYSESR).

in order to reach connect the TMS570 HDK with the CCS but I cannot read the value for SYSESR and the board still does not connect.

I've tried to connect with the Uniflash in order to delete the flash but I cannot connect with the board.

Could you please help me?

  • Hi,

    Apologies for late response. Do you use the board built-in xds100v2 emulator? When you connect the target, what kind of error message did you get?

    The Launchpad built-in emulator is xds110, but HDK is xds100v2. You can not use xds110 for HDK.