Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: UNIFLASH
Good afternoon, everyone. I have a problem that bothers me a lot. I hope you can help me.
I want to set MAC address for TM4C1294NCPDT development board.The MAP_FlashUserSet function and the MAP_FlashUserSave function are used to set MAC address,the
MAP_FlashUserGet function is used to get MAC address.
In TivaWare_C_Series-2.1.4.178\driverlib\rom_map.h:

In TivaWare_C_Series-2.1.4.178\driverlib\flash.c:



My test code is as follows:

When the development board has not written a MAC address, I will pass in a MAC address stored in pdata and set bwrite to true to indicate that I am ready to write to the Mac.Then I processed pdata to get ui32User0 and ui32User1, wrote the MAC address with Map_FlashUserSet, and then saved it with Map_FlashUserSave.When bwrite is set to false, I use MAP_FlashUserGet to get the MAC address and assign it to the structure cMac.cMac is used to display MAC addresses.
My problem is that the first time I write to the MAC address, the data I read with MAP_FlashUserGet is correct.However, when I re-use the MAP_FlashUserSet and MAP_FlashUserSave functions to modify the MAC address, the data I read back is still the same as before.
Map_flashUserSet and map_flashUserSave can only set the MAC address once?How can I solve this problem?Any suggestions from anyone would be most appreciated.