Part Number: TMS570LS3137
Kind Attn
At present, we are using TMS570LS3137 device on the design.
1. The question is regarding the external transceiver mentioned in the document spnu511d.pdf page 42 in the section 6.22.
There is no mention in the Hardware Development kit of the same device. Can you please suggest a device which can be used as external transceiver for the SCI and LIN.
2. The SCI interface is between TMS570LS3137 and custom SoC having 1.8V level Data Input, Data Out, RTS and CTS. Can the RTS and CTS be shorted at the custom IC side, because RTS and CTS pins are not present at the TMS570LS3137.
3. Can the LIN be used in the similar manner to interface to the custom IC UART port as that of SCI, or any extra hardware is required?
Can you please address the above. Thank You.