This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Observed Issue: One or more of PD0, PD1, PB6, and/or PB7 are exhibiting unexpected behavior when trying to use them for any functionality.
Solution: The EK-TM4C123GXL has a pair of zero ohm resistors populated which tie together:
These resistors are used only to support the Airmouse example that works in conjunction with the BOOSTXL-SENSHUB BoosterPack.
They can be removed to allow the GPIO to operate independently as long as that example is not being currently used.