This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: ECLK Output Jitter

Part Number: TMS570LC4357

Hi Team,

My customer noticed on some of their designs that they are using the ECLK output from a TMS570LC4357 MCU as the ethernet transceiver reference clock input (25 MHz). They were able to measure this clock and found that it had a lot of jitter, possibly outside of the PHY transceiver range. 

Do you have the specs (tolerance, jitter, etc.) for this TMS570's ECLK output? I can't seem to find them stated in the spec sheets.

Thanks,
Mitchell

  • Hi Mitchell,

    If PLL is the clock source for ECLK, the jitter of crystal and PLL is also propagated to ECLK pin. The jitter of ECLK output clock is much bigger than the jitter of a crystal. Power supply noise (ground bounce, VCCPLL noise) is the largest contributor to PLL jitter. ECLK is normally used as an indicator of the device operating frequency to check that the device is operating at the correct frequency.

    We don't have the specification of the jitter of ECLK output clock.