Part Number: MSP432P4111
Other Parts Discussed in Thread: SYSBIOS
Hi,
I'm using the idle task for logging data out UART from both LoggerIdle and SysMin, so I need to add a mutex to synchronize the two streams so the data isn't interleaved. This is fine and works well, but I specifically need to use `GateMutexPri` to avoid priority inversion. However, when using this it triggers an assertion when leaving the gate from the idle thread. Specifically, it triggers the following one, from line 1120 in `simplelink_msp432p4_sdk_3_40_01_02/kernel/tirtos/packages/ti/sysbios/knl/Task.c`
Assert_isTrue((((priority == -1) || (priority > 0) ||
((priority == 0 && Task_module->idleTask == NULL))) &&
(priority < (Int)Task_numPriorities)),
Task_A_badPriority);
It is triggered because the idle task's priority is 0, which is only valid for the idle thread.
However, I believe it is fine in this specific case unless I'm missing something. If I'm not, then can we change the assertion to check for this case? e.g.
Assert_isTrue((((priority == -1) || (priority > 0) ||
((priority == 0 && Task_module->idleTask == NULL)) ||
(priority == 0 && tsk == Task_getIdleTask())) &&
(priority < (Int)Task_numPriorities)),
Task_A_badPriority);
Thanks
Campbell