Part Number: UNIFLASH
Other Parts Discussed in Thread: CC1350
I have two CC1350 launchpads that I want to flash with different firmware using the Uniflash CLI (dslite). Both have updated XDS110 firmware and are shown when I run the display-devices script.
If I have only one launchpad connected, the script works fine. If I have both connected, it will select an arbitrary board. How can I specify which device it should connect to?