Part Number: TMS570LC4357
Other Parts Discussed in Thread: LAUNCHXL2-570LC43
Hi,
I hope you've good health during this difficult covid-19 period.
I have downloaded a project which is builted from QJ Wang about the board LAUNCHXL2-570LC43
When I try to load code into the board I got that message :
CortexR5: Loader: One or more sections of your program falls into a memory region that is not writable. These regions will not actually be written to the target. Check your linker configuration and/or memory map.
CortexR5: File Loader: Verification failed: Values at address 0xF0407FF0 do not match Please verify target memory and memory map.
CortexR5: GEL: File: C:\Users\PC_1742_ADMIN\Desktop\Hercules_Ethernet_Bootloader_DELETED\Build-LAUNCHXL2-TMS570LC43x-tftpBoot\Debug\Build-LAUNCHXL2-TMS570LC43x-tftpBoot.out: a data verification error occurred, file load failed.
When I Close de verification a message says like that :
CortexR5: Loader: One or more sections of your program falls into a memory region that is not writable. These regions will not actually be written to the target. Check your linker configuration and/or memory map.
I have changed GJ Wang code as follows in main.c as follows ;
/********************************************************************************************************
*
* main.c : The main file for ethernet bootloader.
* Author : QJ Wang. qjwang@ti.com
* Date : 4-25-2021
*/
/* Copyright (C) 2013-2020 Texas Instruments Incorporated - http://www.ti.com/
*
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the
* distribution.
*
* Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
* "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
* LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
* A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
* OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
* SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
* LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
* DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
* THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*/
/*---------------------------------------------------------------------------------------------------------------------
* Revision History
*---------------------------------------------------------------------------------------------------------------------
* Version Date Author Description
*---------------------------------------------------------------------------------------------------------------------
* 00.10.00 25/04/2021 QJ Wang 1. Initial Version
***********************************************************************************************************/
/* USER CODE BEGIN (0) */
/* USER CODE END */
/* Include Files */
#include "HL_sys_common.h"
/* USER CODE BEGIN (1) */
#include "HL_system.h"
#include "HL_gio.h"
#include "HL_sci.h"
#include "lwiplib.h"
#include "bl_tftp.h"
#include "bl_config.h"
#include "uartstdio.h"
#include "ustdlib.h"
#include "HL_esm.h"
/* USER CODE END */
/** @fn void main(void)
* @brief Application main function
* @note This function is empty by default.
*
* This function is called after startup.
* The user can use this function to implement the application.
*/
/* USER CODE BEGIN (2) */
#define ENABLE_UPDATE_CHECK
#define FORCED_UPDATE_PIN 4
//*****************************************************************************
//
// This holds the current address that is being written to during a download
// command.
//union
//*****************************************************************************
uint32_t g_ulTransferAddress;
uint32_t g_pulUpdateSuccess[8] = {0x5A5A5A5A, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0};
uint32_t g_ulUpdateStatusAddr = APP_STATUS_ADDRESS;
uint32_t g_ulUpdateBufferSize = 32; /*32 bytes */
void IntMasterIRQEnable (void);
void sciDisplayText(sciBASE_t *sci, uint8_t *text,uint32_t length);
uint32_t CheckGPIOForceUpdate(void);
#if 1
extern unsigned int apiLoadStart;
extern unsigned int apiLoadSize;
extern unsigned int apiRunStart;
extern unsigned int constLoadStart;
extern unsigned int constLoadSize;
extern unsigned int constRunStart;
#endif
/* USER CODE END */
uint8_t emacAddress[6] = {0x7C, 0xE6, 0xD3, 0x69, 0x8E, 0xD7};
//*****************************************************************************
//
// Display an lwIP type IP Address.
//
//*****************************************************************************
void
DisplayIPAddress(uint32_t ui32Addr)
{
char pcBuf[16];
//
// Convert the IP Address into a string.
//
#if defined(_TMS570LC43x_)
usprintf(pcBuf, "%d.%d.%d.%d", (ui32Addr >> 24) & 0xff, (ui32Addr >> 16) & 0xff,
(ui32Addr >> 8) & 0xff, (ui32Addr >> 0) & 0xff);
#endif
#if defined(_RM57Lx_)
usprintf(pcBuf, "%d.%d.%d.%d", ui32Addr & 0xff, (ui32Addr >> 8) & 0xff,
(ui32Addr >> 16) & 0xff, (ui32Addr >> 24) & 0xff);
#endif
//
// Display the string.
//
UARTprintf(pcBuf);
}
/* This example works for HDK*/
void main(void)
{
/* USER CODE BEGIN (3) */
unsigned int ipAddr;
g_pulUpdateSuccess[1]= APP_START_ADDRESS;
g_pulUpdateSuccess[3] = 0x20002021; /*version number, 02.00, in 2021*/
esmREG->SR1[0] = 0xFFFFFFFF;
esmREG->SR1[1] = 0xFFFFFFFF;
esmREG->SR1[2] = 0xFFFFFFFF;
esmREG->SR4[0] = 0xFFFFFFFF;
esmREG->EKR = 0x0A;
esmREG->EKR = 0x00;
/* Copy the flash APIs to SRAM*/
memcpy(&apiRunStart, &apiLoadStart, (uint32)&apiLoadSize);
gioInit();
sciInit();
gioSetDirection(gioPORTB, 0xC0);
sciSetBaudrate(UART, UART_BAUDRATE);
/* Enable the interrupt generation in CPSR register */
_enable_IRQ();
UARTprintf("Ethernet lwIP Bootloader \n\r");
uint8 ip_addr[4] = { 192, 168, 0, 2};
uint8 netmask[4] = { 255, 255, 255, 0 };
uint8 gateway[4] = { 192, 168, 0, 3};
bool isProcessDone = false;
bool isPressed = false;
if(((*(uint32_t *) APP_STATUS_ADDRESS) == 0x5A5A5A5A))
{
UARTprintf("ITS ENTER HERE.................................");
g_ulTransferAddress = (uint32_t)APP_START_ADDRESS;
// ((void (*)(void))g_ulTransferAddress)();
}
while (!isProcessDone)
{
if(!gioGetBit(gioPORTB, 4))
{
isPressed = true;
gioToggleBit(gioPORTB, 6);
}
if (!ipAddr)
{
ipAddr = lwIPInit(0, emacAddress,
*((uint32_t *)ip_addr),
*((uint32_t *)netmask),
*((uint32_t *)gateway),
IPADDR_USE_STATIC);
gioSetBit(gioPORTB, 7, 0);
}
else
{
gioSetBit(gioPORTB, 7, 1);
}
UARTprintf("HDK IP Address: ");
DisplayIPAddress (ipAddr);
UARTprintf(" \n\r ");
if(isPressed)
{
break;
// isProcessDone = true;
// isPressed = false;
// gioSetBit(gioPORTB, 6, 0);
// gioSetBit(gioPORTB, 7, 0);
}
}
TFTPQSInit(); // If the isPressed ( TO BUTTON GPIOB_4 EXIT FROM WHILE LOOP AND COMES HERE. )
UARTprintf("DONE ");
}
void sciDisplayText(sciBASE_t *sci, uint8_t *text,uint32_t length)
{
while(length--)
{
while ((sci->FLR & 0x4) == 4);
sciSendByte(sci,*text++);
};
}
void IntMasterIRQEnable(void)
{
_enable_IRQ();
return;
}
void IntMasterIRQDisable(void)
{
_disable_IRQ();
return;
}
unsigned int IntMasterStatusGet(void)
{
return (0xC0 & _get_CPSR());
}
/*
** Interrupt Handler for Core 0 Receive interrupt
*/
volatile int countEMACCore0RxIsr = 0;
#pragma INTERRUPT(EMACCore0RxIsr, IRQ)
void EMACCore0RxIsr(void)
{
countEMACCore0RxIsr++;
lwIPRxIntHandler(0);
}
/*
** Interrupt Handler for Core 0 Transmit interrupt
*/
volatile int countEMACCore0TxIsr = 0;
#pragma INTERRUPT(EMACCore0TxIsr, IRQ)
void EMACCore0TxIsr(void)
{
countEMACCore0TxIsr++;
lwIPTxIntHandler(0);
}
//*****************************************************************************
//
// Checks a GPIO for a forced update.
//
// This function checks the state of a GPIO to determine if a update is being
// requested.
//
// \return Returns a non-zero value if an update is being requested and zero
// otherwise.
//
//*****************************************************************************
#ifdef ENABLE_UPDATE_CHECK
uint32_t
CheckGPIOForceUpdate(void)
{
/** bring GIO module out of reset */
gioREG->GCR0 = 1;
gioREG->ENACLR = 0xFF;
gioREG->LVLCLR = 0xFF;
// Set the pin as input
gioPORTA->DIR &= ~(1 << FORCED_UPDATE_PIN);
// Enable the pull up/down.
gioPORTA->PULDIS &= ~(1 << FORCED_UPDATE_PIN);
// Enable the weak pull up.
gioPORTA->PSL |= 1 << FORCED_UPDATE_PIN;
// Check the pin to see if an update is being requested.
if ((gioPORTA->DIN & (0x1 << FORCED_UPDATE_PIN) ) == 0)
{
// Remember that this was a forced update.
return(1); //force to update
}
// No update is being requested so return 0.
return(0);
}
#endif
/* USER CODE END */