Part Number: LM3S3739
We are using receive interrupt, for receiving packet details, but it works with only FIFOLevelSet.
We need receive interrupt trigger for single byte,
We checked with UARTFIFO disable option also, but receive interrupt is occurring for 8 bytes, not occurring for single byte.
how to handle please suggest me.
Currently we are using the below setting for UART Receive
UARTHandler()
ulStatus=UARTIntStatus(UART2_BASE,1);
UARTIntClear(UART2_BASE,ulStatus);
while(UARTCharsAvail(UART2_BASE))
{
rs485.rx_buffer[rs485.rx_count]=UARTCharGet(UART2_BASE);
rs485.rx_count++;
}
FIFOLevel setting
UARTFIFOLevelSet(UART2_BASE,UART_FIFO_TX1_8,UART_FIFO_RX1_8);
With the above settings, we are receiving the interrupt for every 2 bytes.
We need to receive interrupt for every 1 byte.