Part Number: TM4C129ENCPDT
Other Parts Discussed in Thread: EK-TM4C129EXL
Hi,
I have designed a TM4C129ENCPDT based board. The board design is based on EK-TM4C129EXL. A couple of proto boards are ready for testing. I also have Installed the TivaWare and are using the Project0 for checking the initial programming/debugging and then port pin toggling. The project is built properly with no errors. When I try to debug the code I am getting an below error:
CORTEX_M4_0: Error Initializing flash programming: Target Failed to read 0x400fE000. Below is the screenshot of the error: