Part Number: MSP432E401Y
Here is how I plan to initialize 2 SPI buses on SSI0 and SSI2
First: is this the right way to do this!
- I plan to open 2 SPI ports on init and keep them open through the lifetime of the board. Do I need to check if the connection is open after a while?
- I plan to use CA_SPI_WRITE to read and write using one of those 2 SPI ports
- Because I used syscfg GUI to set up SPI I don't have access to the CS pin of either SPI port DIRECTLY
- Is there a way of toggling those CS pins from another function? rephrase (how can I access those CS pins without affecting the way I wrote (spiBus_Init)?
void spiBus_Init()
{
/* Initialize SPI handle as default master */
SPI_init();
SPI_Params_init(&masterSpiParamsCa);
SPI_Params_init(&masterSpiParamsEis);
memset(masterRxBufferCa, 0, sizeof(masterRxBufferCa));
memset(masterTxBufferCa, 0, sizeof(masterTxBufferCa));
memset(masterRxBufferEis, 0, sizeof(masterRxBufferEis));
memset(masterTxBufferEis, 0, sizeof(masterTxBufferEis));
masterSpiParamsCa.frameFormat = SPI_POL0_PHA1;
masterSpiParamsCa.bitRate = 10000000;
masterSpiParamsCa.mode = SPI_MASTER;
masterSpiParamsCa.dataSize = 8;
masterSpiParamsCa.transferCallbackFxn = CatransferCompleteFxn;
masterSpiParamsEis.frameFormat = SPI_POL0_PHA1;
masterSpiParamsEis.bitRate = 10000000;
masterSpiParamsEis.mode = SPI_MASTER;
masterSpiParamsEis.dataSize = 8;
masterSpiParamsEis.transferCallbackFxn = EistransferCompleteFxn;
masterSpiCa = SPI_open(CONFIG_SPI_CA, &masterSpiParamsCa);
if (masterSpiCa == NULL) System_abort("Error initializing CA master SPI\n");
else printf("Master CA SPI initialized\n");
masterSpiEis = SPI_open(CONFIG_SPI_EIS, &masterSpiParamsEis);
if (masterSpiEis == NULL) System_abort("Error initializing EIS master SPI\n");
else printf("Master EIS SPI initialized\n");
//SPI_control(spiHandle, SPICC26XXDMA_RETURN_PARTIAL_ENABLE, NULL); // ??
}
Here is the block to Readorwrite using the handle from above:
uint8_t CA_SPI_WRITE(uint8_t nBytes, uint8_t* txBufferPointer, uint8_t* rxBufferPointer, uint8_t CS_pin){
/* Copy message to transmit buffer */
strncpy((char *)masterTxBufferCa, MASTER_MSG, SPI_MSG_LENGTH);
uint8_t i;
for (i = 0; i < MAX_LOOP; i++)
{
// Initialize master SPI transaction structure
masterTxBufferCa[sizeof(MASTER_MSG) - 1] = (i % 10) + '0';
memset((void *) masterRxBufferCa, 0, SPI_MSG_LENGTH);
masterTransactionCa.count = SPI_MSG_LENGTH;
masterTransactionCa.txBuf = (void *)masterTxBufferCa;
masterTransactionCa.rxBuf = (void *)masterRxBufferCa;
// Turn on user LED, indicating a SPI transfer is in progress
GPIO_write(CONFIG_LED_ORANGE_GPIO, CONFIG_GPIO_LED_ON);
// Initiate SPI transfer
bool transferOK = SPI_transfer(masterSpiCa, &masterTransactionCa);
if (transferOK) printf("Master: %s\n", masterRxBufferCa);
else printf("Unsuccessful master SPI transfer");
// Sleep a short time to allow the LED to flash
usleep(500000);
// Turn off user LED, indicating the SPI transfer is done
GPIO_write(CONFIG_LED_ORANGE_GPIO, CONFIG_GPIO_LED_OFF);
// Sleep for a bit before starting the next SPI transfer
sleep(3);
// should i close the spi ?
}
return 0;
}