Part Number: TMS570LS3137
Hello all,
I am new using HDK TMS570LS3137, I want to write a data to an address from one SPI to another.
SPI3 is going to be TX, SPI1 RX.
Then, copied these codes,
#define SPI3_TX_ADDR ((uint32_t)(&(spiREG3->DAT1)) + 2)
#define SPI1_RX_ADDR ((uint32_t)(&(spiREG1->BUF)) + 2)
unsigned int BlockSize = 100;
unsigned short TX_DATA[100];
unsigned short RX_DATA[100] = {0};
dmaConfigCtrlRxPacket(SPI1_RX_ADDR, (unsigned int)&RX_DATA, 1, BlockSize);
dmaConfigCtrlTxPacket((unsigned int)&TX_DATA, SPI3_TX_ADDR, 1, BlockSize);
and some others as well.
Now, I want to write a data to an address and I don't know how to do it. Should I use ISADDR, IDADDR registers or something.
For example, I just wrote these
for(i=0; i< BlockSize; i++)
{
TX_DATA[i] = i;
}
and want it to write on an address. I mean, from TX to RX.
Need your help, best wishes.
Caner