Hi,
The nTRST connection diagram included in the Hercules development kit is shown in Image-1.
Based on this connection, a connection is made from the 3V3 voltage supply to the MCU nTRST pin through the 4K7 resistor (Image-2). The software load could not be done while there was no change in the current drawn by the MCU.
Then, a direct connection was established with the MCU nTRST pin from the 3V3 voltage supply (Image-3). When current measurement is made between nTRST and 3V3, it is seen that it draws 120mA current. Software loaded successfully despite high current draw.
There is no current value information about the nTRST pin in the MCU datasheet. My question is, what effect does the 120mA seen between the MCU nTRST and the 3V3 voltage source have on MCU health? How can I solve this high current draw problem?
Thanks in advance.