Part Number: TMS570LS0432
Hi,
I would like to understand better how to assert properly the nPORRST pin:
- To activate the nPORRST, it must be pulled down to gnd. What would be the nominal voltage for the Pull-up? Vccio voltage?
- From timing perspective, nPORRST must be active at least 1ms, until both Vccio and Vcc reach Vccporh and Vccioporh voltages. Is this correct?
- From timing perspective, it is shown in the figure 6-1 of the datasheet that nPORRST must be active low before Vcc or Vccio goes below the thresholds Vccporh and Vccioporh. Is this indicating that the voltage of the power lines go low after nPORRST is asserted or does this indicate that the reset needs to be activated before there is an undervoltage?
The idea would be to supply the uC with 2 LDOs, and we would like to implement some comparators that monitor Vcc and Vccio voltages. In case of out of the recommended range, they would trigger the nPORRST. Do you have a similar application diagram?
Any other consideration required to implement correctly the reset?
Thank you in advance.