Part Number: MSP432E401YT
Other Parts Discussed in Thread: MSP432E401Y, UNIFLASH
- I recently built a board with MSP432E401Y MCU
- However, the MCU was out of stock everywhere so I removed one from MSP432E4 Launchpad and installed it on my custom board.
- I am using the XDS110 on board debugger to program my custom board.
- Using PC0, PC1, PC2, PC3 to program my custom board and the circuit and jumpers look good (schematic below)
- Custom board connected to XDS110 using
- TCK, TMS, TDI, TDO & TARGET_RESET



Initially I was getting ERROR: Error -615, Target failed to see a correctly formatted SWD header
- Did some research and found out that because I took the MCU out of a launchpad it might be in production mode so I tried to factory reset it using
- “Unlock Sequence Using Uniflash and XDS Debug Probes”
- "dbgjtag.exe –f @xds110 –Y unlock,mode=msp432e4"
Anyway i noticed that the Analogue Voltage was not connected so after turning that on Error -615 went away
Now when i test connection with these configs in ccxml i get:
[Start: Texas Instruments XDS110 USB Debug Probe]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\UTKARS~1.GUP\AppData\Local\TEXASI~1\
CCS\ccs930\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioxds110.dll'.
The library build date was 'Nov 25 2019'.
The library build time was '16:55:29'.
The library package version is '8.4.0.00006'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '5' (0x00000005).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.
-----[Print the reset-command hardware log-file]-----------------------------
The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the XDS110 with USB interface.
The link from controller to target is direct (without cable).
The software is configured for XDS110 features.
The controller cannot monitor the value on the EMU[0] pin.
The controller cannot monitor the value on the EMU[1] pin.
The controller cannot control the timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '0' (0x0000).
-----[Perform the Integrity scan-test on the JTAG IR]------------------------
This test will use blocks of 64 32-bit words.
This test will be applied just once.
Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Scan tests: 2, skipped: 0, failed: 0
Do a test using 0xFE03E0E2.
Scan tests: 3, skipped: 0, failed: 0
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 0
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 0
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 0
All of the values were scanned correctly.
The JTAG IR Integrity scan-test has succeeded.
-----[Perform the Integrity scan-test on the JTAG DR]------------------------
This test will use blocks of 64 32-bit words.
This test will be applied just once.
Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Scan tests: 2, skipped: 0, failed: 0
Do a test using 0xFE03E0E2.
Scan tests: 3, skipped: 0, failed: 0
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 0
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 0
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 0
All of the values were scanned correctly.
The JTAG DR Integrity scan-test has succeeded.
[End: Texas Instruments XDS110 USB Debug Probe]

When I try to debug (program the MCU):
CORTEX_M4_0: GEL_OUTPUT:
Memory Map Initialization Complete
CORTEX_M4_0: Jtag Communication Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.4.0.00129)
CORTEX_M4_0: Failed to remove the debug state from target before disconnecting.
Not sure what to do here, please help!
- i tried lowering the TCLK to 2.5MHz but the problem still persists!